Anixter: Products & Technology
   Contact Us Websites by Country Site Search (Tips)  
 Anixter logo  USA
  
    
 
  
   Sort by:
> Overview
> Enterprise Cabling Solutions
> Security Solutions
> Electrical and Electronic Wire & Cable
> Fasteners and 'C' Class Components
> Manufacturers (+/-)
> Case Studies


 Find products:   

 View your Account:   

1.800.ANIXTER in U.S.
 I wish to be contacted
 by an Anixter expert

Products >> Enterprise Cabling Solutions
Network Powered Solution for Campus Safety Provides Visual Emergency Messaging to Critical Campus Locations


Inova Solutions LED displays available through Anixter to increase campus safety

Richmond, VA – August 4, 2008 – From the Governor’s Campus Preparedness Conference, Inova Solutions, Inc. announced that its OnAlert™ mass notification system, which is a new campus security solution that displays alerts on network-powered LED signs, will be installed at Virginia Tech University. These highly visible LED displays are powered by a single network connection using standard Power over Ethernet (PoE) technology to provide both power and data to the displays.

Virginia Tech has purchased 220 OnAlert displays to deliver focused information to the university’s classrooms and teaching spaces. The displays will provide continuous value as they display the time and date when there are no messages to present.

OnAlert provides an easy but secure way for authorized school officials to issue emergency alerts on LED displays. “The OnAlert displays are visible from over 100 feet and the Power over Ethernet design allows them to operate on only 12 watts of power,” said Gerry Gorman, Vice President at Inova Solutions. “The low-energy usage makes them a ‘green’ product that is inexpensive to install and operate.”

The OnAlert displays for the Virginia Tech project were purchased through Anixter (www.anixter.com, 1-800-ANIXTER). “Anixter is excited to be part of a project that incorporates Power over Ethernet technology into campus safety and security solutions,” said Brent Streetman, Vice President Marketing – Security Solutions. "As organizations continue to update and enhance their security systems, we look for new, innovative products to add to our portfolio to assist them with their efforts. We feel the product features of Inova’s OnAlert displays are of particular value as customers migrate their security systems to Ethernet networks.”

OnAlert Power over Ethernet (PoE) LED Displays
Inova Solutions’ OnAlert PoE LED displays deliver synchronized time, non-emergency and emergency messages across a campus in one simple appliance. They plug directly into a standard Ethernet jack to obtain messaging, time and power from a single network connection, so no AC outlets are needed. The system can support redundant power via a UPS in the communications room, and because the same network is used for both control and power, Power over Ethernet devices minimize installation and maintenance costs by delivering power through high-performance twisted-pair data cabling systems, rather than dedicated 120 VAC hard-wired connections. Messages can also be sent to the displays via Inova’s Emergency Email Interface (EEI) software. These PoE appliances carry the CE Mark and are RoHS compliant. Learn more about Inova’s OnAlert mass notification system at http://www.inovasolutions.com/products/on-alert.html


About Anixter
Anixter International is a leading global distributor of communication products, electrical and electronic wire and cable and fasteners and other small parts. The company adds value to the distribution process by providing its customers access to 1) innovative inventory management programs; 2) more than 400,000 products and $1 billion in inventory; 3) 214 warehouses with more than 6 million square feet of space; and 4) locations in 248 cities in 50 countries. Founded in 1957 and headquartered near Chicago, Anixter trades on The New York Stock Exchange under the symbol AXE.

- ### -




Media Contacts:

Dawn Marks, dawn.marks@anixter.com, 224-521-8484
Gerry Gorman, ggorman@inovasolutions.com, 434-951-8212


Check Inova's OnAlert disply in our e-catalog!

Corning Cable Systems Announces Significant Web Page Enhancements 2008-10-29
The Web page improvements streamline site organization and navigation while creating a strong foundation for more refinements to the site in the coming years.

Corning Demonstrates Leadership in High-Data-Rate, Parallel Optic Transmission 2008-09-16
Corning to feature 40G performance capability at Interop New York

Greenlee's Sidekick Series 2008-09-05
Greenlee's Sidekick series has become a benchmark in communications technology-- light-weight, hand-held meters that quickly and accurately uncovers intermittent troubles that other test sets can’t detect.

JDSU Resi-Tracer TT300 2008-09-05
A triple-function tone tracer with speaker phasing and telephone line monitoring capabilities.

Power Recording and Analysis Techniques and Applications 2008-08-08
Hooking up a power quality recorder and taking days’ worth of data can give you a rich picture of your power. What should you be looking for? And when does recording make sense?

Network Powered Solution for Campus Safety Provides Visual Emergency Messaging to Critical Campus Locations 2008-08-08
Inova Solutions LED displays available through Anixter to increase campus safety

Fluke 1750 Three-Phase Power Recorder 2008-07-10
Capture every measurement, every event, on every cycle, all the time with the Fluke 1750 Power Recorder. Unprecedented accuracy and resolution provide complete visibility into your distribution system.

Greenlee's Low Voltage Electrical Kit 2008-07-10
A complete package for low voltage applications.

Corning Cable Systems Introduces OTS-600 Series for Simplified Optical Network Certification in LAN Applications 2008-07-09
Corning Cable Systems LLC introduces its new OTS-600 Series optical sources, meters, testers and kits with data storage capabilities.

Corning Cable Systems Introduces Fusion Splicer for the Next Generation of LAN Applications 2008-07-09
Corning Cable Systems LLC introduces its new OptiSpliceŽ M90e Fusion Splicer, a feature-rich machine for networks where low-loss performance and high-end accuracy are imperative.


[Entries 1 - 10] of [71]
Next

 

<<Back E-mail this Page to a Colleague>>  Printer Friendly Format

   
  Privacy Statement  |  Terms & Conditions  |  Contact Us  |  Investor Relations  |  ©2007 All Rights Reserved  |